WITTENSTEIN at LogiMAT 2024
From March 19 to 21, 2024, WITTENSTEIN cyber motor will be unveiling the new cyber® simco® drive 2, a safety certified servo drive with a PROFIsafe interface, at the LogiMAT trade show in Stuttgart (Hall 6, Booth 6B04). This safe fieldbus interface is available for the SIM2050 and SIM2100 output variants with an integrated safety board. In combination with the drive actuator, these are used in the compact cyber® iTAS® system 2 servo drive system for automated guided vehicles (AGVs).
The PROFIsafe interface of the servo drives makes an important contribution to the compact AGV drive system’s next-level safety architecture by reducing the complexity of the safety and control technology in the vehicles as well as the time and costs for commissioning and servicing. It also simplifies the configuration and documentation of the safety architecture. There are plans to implement more safe interfaces in the cyber® simco® drive 2 servo drive later in 2024.
Safe communication for AGVs, AMRs & co. enables cost-effective vehicle design
When equipped with an integrated safety board, the cyber® simco® drive 2 servo drive has a two-channel STO (Safe Torque Off) function even in the basic version. Safe Brake Control (SBC) and Safe Position (SP) safety functions as well as an emulation for the safety encoder in the wheel actuator can be optionally integrated.
Thanks to the PROFIsafe interface in the servo drive’s SIM2050 and SIM2100 output variants, manufacturers of AGVs and AMRs (autonomous mobile robots) can now design and implement their vehicle safety architecture even more easily and cost-effectively. The safe signals from the servo drive to the safety and vehicle control system are transmitted via a safety certified communication channel – eliminating the need for additional wiring or for a second channel for speed and position monitoring.
Overall, the safety certified cyber® simco® drive 2 PROFIsafe servo drive – and with it the cyber® iTAS® system 2 AGV drive system – meets SIL 2 and PL d requirements as stipulated by the majority of vehicle manufacturers and operators.
PROFIsafe interface supports next-level safety architecture
PROFIsafe is a standard for a communication protocol for the transmission of safety-relevant data via PROFINET or PROFIBUS in automation applications with functional safety. The technology – according to the PROFIBUS and PROFINET International Support Centre (PISC) in Karlsruhe, almost seven million nodes are meanwhile installed in the field – covers the entire communication path from the sensor to the controller and the actuator.
As a standard within IEC 61784-3-3, it integrates both safety and standard communication technology on one cable – ideally supporting the next-level safety architecture developed by WITTENSTEIN for the safety certified cyber® simco® drive 2 servo drive, as used in the cyber® iTAS® system 2, the compact drive system for AGVs. The safety architecture for AGVs, AMRs and other mobile platforms requires fewer cables and connectors, fewer interfaces, components and modules and reduces assembly and documentation effort – without in any way compromising safe AGV and AMR operation.
The WITTENSTEIN group at LogiMAT 2024
Frameless motors from WITTENSTEIN cyber motor enabling in-house development of actuators for AGVs and AMRs as well as small servo drive systems for auxiliary axes will be further highlights at the LogiMAT booth. WITTENSTEIN alpha will additionally be presenting planetary, bevel and worm gearboxes along with rack-and-pinion applications for material handling, among others.
For more information on the cyber® iTAS® system 2 drive system, go to: www.wittenstein-itas.com/en
Pictures (source: WITTENSTEIN SE)
Photo01: 01-wittenstein-fts-antriebssystem
cyber® iTAS® system 2, the AGV drive system comprised of an actuator and a servo drive. It combines a lean and integration-friendly safety architecture with maximum power density, giving the vehicles a decisive gain in performance and increasing productivity.
Photo 02: 02-wittenstein-fts-servoregler
The cyber ® simco® drive 2 servo drive with IP65 protection is the perfect solution for AGVs, AMRs and other mobile platforms. The drive is now also available with a PROFIsafe interface.
Photo 03: 03-wittenstein-fts-antriebssystem
The cyber ® iTAS® system 2 drive system for AGVs enables high-performance differential drives to be implemented with only 180 mm of mounting space under the body, vehicle widths of just 460 mm and vehicle masses between 1 and 3 tons.