Pioneers set new benchmarks – again!
Setting new technology benchmarks means raising the bar in the market. This is something WITTENSTEIN has been doing for more than thirty years now with astounding regularity.
Gear design: low-backlash and backlash-free innovations
When the first low-backlash SP planetary gearheads were manufactured by WITTENSTEIN alpha back in 1983, a new era dawned for decentralized drive technology – away from a central line shaft. Since then, more than two million low-backlash planetary gearheads have come off the production line. The newest high speed version, the SP+ HIGH SPEED, currently sets the benchmark in applications where maximum positioning accuracy and speeds are essential during continuous operation. Low backlash, optimal torsional rigidity and high precision – these three outstanding attributes of the hypoid gearheads redefined the technological standard when the series was unveiled back in 2007.
In spring 2015, WITTENSTEIN took the leap from low-backlash to backlash-free with the Galaxie Drive System – another highlight among the exhibits at this year's Motek. It's the completely redesigned kinematic principle without a gear wheel that sets Galaxie apart from the rest: each tooth is an independent and dynamic entity, so that full surface contact takes place, not line. As a result of this optimized engagement, Galaxie beats all conventional gearhead types in all important technical details.
Focus on customer and industry needs: "no compromise" approach
Two years previously in 2013, WITTENSTEIN alpha launched the world's first planetary gearhead with EHEDG1 certification, which caters for the needs of machine builders and plant operators in the food processing and packaging industry. The HDV and HDP Hygienic Design gearheads with an output shaft or output flange which be on show at Motek put an end to the typical compromises as regards the choice of materials, component design or type of enclosure with a combination of optimal sealing properties against fluid ingress or discharge, incomparable resistance to corrosion owing to the special hygienic steel and easy-to-clean housing surfaces. The outcome: hygienic machine designs as well as safer processing, filling and packaging with no microbial contamination or other product risks.
Innovative rack installation: intelligent integration
It isn't just the performance features with which WITTENSTEIN sets benchmarks again and again. Innovative ideas are often inspired by drive solutions that have proven successful in practice. Our integrated rack installation technique is a good case in point. Instead of the traditional method of first fixing the racks to a machine bed with screw clamps and then bolting them tight, WITTENSTEIN racks can now be mounted directly and highly precisely thanks to an integral clamping device. This revolutionary system enables assembly times to be reduced by up to 50%.
Maintenance without downtime: optimal availability for linear actuators
The cyber force motors made by WITTENSTEIN cyber motor convert rotational into linear movements. Over and above this basic function, these linear actuators open up a range of exciting solutions due to their individual design and high power density. This is true both in everyday industrial use and in rough environmental conditions. Featuring a highly integrated ball screw, the linear actuators set benchmarks with a novel feature that creates genuine added value and dramatically improves serviceability: owing to the patented lubrication system, the screw can be regreased during operation without having to stop the machine for maintenance. Maintenance-free solutions can also be developed on request.
The pioneers at WITTENSTEIN set new benchmarks again and again – with the constant new challenges presented by the market for the Group's product and service portfolio as the bar for future technological innovations.
EHEDG: European Hygienic Engineering & Design Group
Photos:
1. The newest high speed version, the SP+ HIGH SPEED, currently sets the benchmark in applications where maximum speeds are essential during continuous operation.
2. In spring 2015, WITTENSTEIN took the leap from low-backlash to backlash-free with the Galaxie Drive System.
3. Two years previously in 2013, WITTENSTEIN alpha launched the HDV / HDP, the world's first Hygienic Design planetary gearheads with EHEDG1 certification, which cater for the needs of the food processing and packaging industry.
4. With the cyber force motors family of linear actuators from WITTENSTEIN cyber motor the ball screw can be regreased during operation – without having to stop the machine for maintenance.